EcoStruxure Process Expert Support Portal

Schneider Electric Industry Business - Digital Plant Line of Business is happy to announce you the availability of the new version of Process Expert.
Please find below detailed information about the new features:

Architectural Extensions

  • Support of the common Safety with Modicon M580 Safety. Address process and safety loops within the same configuration environment to reduce the cost of ownership

High reliability for Online Modifications

  • Safe and reliable on-line modifications of the M580 hardware configuration to reduce the downtime and adapt faster to production requirements.

Engineering Extension and Productivity Improvements

  • Asset interoperability with a workspace to interconnect the plant assets. It increases the productivity in engineering and eases the building reusable process strategies.
  • Auto-assign objects instances in the supervision project to reduce the engineering effort and avoid inconsistencies.

Audit Trail

  • Centralized Audit trail in Engineering to log the changes in the platform and the controller applications. Traceability of activities done off-line/on-line to support regulations.

 Extended hardware module support

  • M580 Safety Controller Range of CPU, Racks and IO Modules
  • X80 Advanced RTU module step 2.1 (BMENOR2200H) module

EcoStruxure Process Expert 2020 R2 is bundled with two libraries

  • A new General-Purpose Library to design applications compliant with Situational Awareness principles.
  • The classic GPL is also embedded in the release