EcoStruxure Process Expert Support Portal

Schneider Electric Industry Business - Digital Plant Line of Business is happy to announce you the availability of the new version of Process Expert.
Please find below detailed information about the new features:

 

Faster System Engineering

  • 35% to 40% less time to add a new asset in the application, from assignment to deployment in a controller.

New communication capabilities

  • Support of OPC UA Server Expert and embedded OPC UA server in a X80 module for more secured communication between controllers and supervision.

Extended hardware support

  • BME NUA100 modules (embedded OPC UA for M580)
  • BMX ERT 1604.2 module

EcoStruxure Process Expert 2020 is bundled with two libraries

  • General-Purpose Library to design applications compliant with Situational Awareness principles. Several object templates have been added.
  •  “Classic” GPL is also embedded in the release.