EcoStruxure Process Expert Support Portal

Schneider Electric Industry Business - Digital Plant Line of Business is happy to announce you the availability of the new version of Process Expert.
Please find below detailed information about the new features:

Architectural Extensions

  • Support of the common Safety with Modicon M580 Safety. Address process and safety loops within the same configuration environment to reduce the cost of ownership

High reliability for Online Modifications

  • Safe and reliable on-line modifications of the M580 hardware configuration to reduce the downtime and adapt faster to production requirements.

Engineering Extension and Productivity Improvements

  • Asset interoperability with a workspace to interconnect the plant assets. It increases the productivity in engineering and eases the building reusable process strategies.
  • Auto-assign objects instances in the supervision project to reduce the engineering effort and avoid inconsistencies.

Audit Trail

  • Centralized Audit trail in Engineering to log the changes in the platform and the controller applications. Traceability of activities done off-line/on-line to support regulations.

 Extended hardware module support

  • M580 Safety Controller Range of CPU, Racks and IO Modules
  • X80 Advanced RTU module step 2.1 (BMENOR2200H) module

EcoStruxure Process Expert 2020 R2 is bundled with two libraries

  • A new General-Purpose Library to design applications compliant with Situational Awareness principles.
  • The classic GPL is also embedded in the release

Schneider Electric Industry Business - Digital Plant Line of Business is happy to announce you the availability of the new version of Process Expert.
Please find below detailed information about the new features:

 

Faster System Engineering

  • 35% to 40% less time to add a new asset in the application, from assignment to deployment in a controller.

New communication capabilities

  • Support of OPC UA Server Expert and embedded OPC UA server in a X80 module for more secured communication between controllers and supervision.

Extended hardware support

  • BME NUA100 modules (embedded OPC UA for M580)
  • BMX ERT 1604.2 module

EcoStruxure Process Expert 2020 is bundled with two libraries

  • General-Purpose Library to design applications compliant with Situational Awareness principles. Several object templates have been added.
  •  “Classic” GPL is also embedded in the release.

Schneider Electric Industry Business - Digital Plant Line of Business is happy to announce you the availability of the new version of Process Expert for AVEVA System platform

EcoStruxure Process Expert for AVEVA System Platform is a Process Automation System to design, engineer, operate and maintain standardized control systems based on Modicon controllers, and provides a seamless Integration with AVEVA System Platform.

 

Reduce Engineering costs

  • Asset Centric System with object oriented and hardware abstraction configuration. The supervision application objects and the hierarchy are automatically created, based on the Plant Asset configuration.
  • Management of Controller communications with AVEVA System Platform
  • Guarantees the system consistency and reduces errors during configuration and maintenance
  • Includes a ready-to-use Process Automation Library (GPL) for Control and the Supervision; includes the capability to design custom application objects.
  • Compatible with AVEVA System platform 2020 with Operations Management Interface (OMI)

Schneider Electric Industry Business - Digital Plant Line of Business is happy to announce you the availability of the new version of EcoStruxure Hybrid DCS.
Please find below detailed information about the new features:


New process automation library based on Situational Awareness:

  • Situational awareness increases the operational efficiency and contributes to run the plant at the peak performance, by helping operators to detect abnormal situation before alarms occur and reducing the time to overcome abnormal situation.

Object instantiation is improved to ease the engineering of the application.

  • Export and Import of folders, instances and application interface links in comma-separated (CSV) file format can be possible.
  • The notification pane logs the changes in the application and the detected issues during import.
  • The Links Editor embeds new services such as Radar View, the simplified view, moving links to a different destination interface, and the possibility to drag several instances to the workspace and position them.
  • The instance validity and progress indicators give you an indication of the steps that remain to complete the instantiation and assignment stages. Write-lock indicators let you see which instances are being used or modified by other processes or users.

New Project Explorer User Interface that maximizes to navigation and edition

  • Separate tree views for Control and Supervision projects, with a multi-tabs workspace area for edition
  • The Last Action Summary command lets you see which is the last action that was performed and its result
  • Validity and progress indicators help designers to complete the system engineering life cycle till deployment stage.

 

Extended services to assign objects instances to projects

  • For Control projects, a powerful editor lets you create your own section names and define assignment strategies for assigning the facets in bulk. You can preview the assignments before proceeding.
  • You can perform actions on several containers at once in the Assignment Editor.

Bulk hardware mapping

  • The functionality to export and import hardware mappings have been enhanced and integrated into the Hardware Mapping Editor making it easy-to-use. The comma-separated (CSV) file from export can be edited to create or modify mappings.
  • The Unmap command now lets you delete all or a selection of hardware mappings.

 

Improved Global Template Management to customize or design an object template

  • The new Duplicate command lets you create a copy of a template with identical and/or different child templates without having to edit it.
  • You cannot update, modify, duplicate or save templates whose identifier contains the $ prefix and keep using this prefix. The use of $ prefix is reserved for global templates that are created by Schneider Electric.
  • The Composite Editor and Facet Editor feature has several improvements, which increase productivity and ease of use
  • In general, the global template editor is improved for better engineering with below features
    • Undo and redo commands
    • Radar view
    • Simplified view to get the template structure at a glance
    • Improved binding management with graphical links and connectors
    • $FullNameproperties to link template elements easier

 

Extension of the architectures with new modules and services

  • The Profibus master module PMEPXM0100 is configured through the Topological Manager. The configuration of the field bus and the devices is required through a separate software (ProSoft Configurator for Modicon).
  • Support of new digital modules
  • You can configure the DHCP service for Ethernet modules into the topology explorer.

 

Miscellaneous enhancements

  • A new command lets you create a blank database at any point in time.
  • The Processor Count parameter is added to the Virtual Machine section of the configuration wizard to adjust the performance of VM-related operations depending on the computer specifications.
  • The generation process of a Control project doesn’t abort when a section cannot be generated (overcrowded size).
  • A button to view asset-related information in the Operation client is now available in the faceplate of genies. It avoids the need for a keyboard when using runtime navigation services. The button is readily available only for new GPL templates of libraries that support it and can be added manually to user-designed templates

 

Schneider Electric Software Update (SESU) is installed as part of EcoStruxure Hybrid DCS software Installation

  • This tool eases the management of software updates. This will be the new way of delivering hotfixes and new version release updates of EcoStruxure Hybrid DCS.

 

Extension of the Foundation Library with new templates

  • A set of Foundation Templates are delivered to extend the capability to design objects
    • Equipment element: Flexibility in defining the required equipment name with all other properties of an equipment to achieve the Situational Awareness capabilities of Citect Scada 2018.
    • Calculated Variable Tag element: It generates a tag value at runtime that is the result of a Cicode expression or a Cicode function.
    • Variable Disk Tag element: Templatize & generate the variable disk tag so that user can get the benefit of using a Disk IO device.
    • Equipment Parameter element: Equipment Parameters element enables to define other complementary information which will help the next generation of Libraries during Runtime and benefit from such new capabilities of Citect Scada
    • Equipment Group of Messages element: Is a set of runtime parameter entries which can accommodate up to 8 messages per group.
    • ItemName property in elements of Supervision data facets: the property is used by Supervision resources with the equipment name to reference controller data, which can be used as a reference for animation and other purposes.

 

General Purpose Library (GPL) 

  • EcoStruxure Hybrid DCS 2019 includes the General-Purpose Library “Classic” and the new General Purpose Library (Situational Awareness).


EcoStruxure Hybrid DCS2018 release R2

   Software Downloads:

     Iso install file

     Blank Data base

   

   Hotfixes

     EcoStruxure Hybrid DCS 2018 for General purpose library Hotfix RTM_51332

          Issue : 50943 : HDCS 2018- General Purpose Libraray - SGC_Include - Standby Server Trend status does not update.

     EcoStruxure Hybrid DCS - MMM Library 2018 Hotfix RTM_51101

          Issue: # 50613: HDCS- 2018- MMM Library- PIDB- Manual mode Manual SP not moved to MV

     EcoStruxure Hybrid DCS MMM Library 2018 Hotfix RTM_46321

          Issue1: # 47516 MMM_Tools Operator Events and Bypass List is only available for one day

          Issue2: # 49579 MMM Tools Bypass List is not working in Multi-Language in specific use case

  

   Documentation

     EcoStruxure Hybrid DCS 2018 R2 Release Notes Platform

     EcoStruxure Hybrid DCS Virtualization Application Note eng EIO0000003796 00

     User guides & manuals updated

 

PES V4.3
   Hotfixes         

     PES 4.3 SP1 RTM_Hotfix 51989

          This hotfix resolves the issue related to StandbyWrite for IODevices in Supervision Project Configuration

 

Knowledge base: 260 FAQs available
    + 7 text FAQs (since last 3 month)

    + 3 video FAQs (since last 3 month)

Text FAQs:

FA365830

EcoStruxure Hybrid DCS [2018]: What are the built in historian capabilities of a Hybrid DCS (PES) application

FA364420

EcoStruxure Hybrid DCS [2018]: No folder to instantiate a template in Application Explorer after installing HDCS 2018 R2

FA363642

EcoStruxure Hybrid DCS [2018]: Failed to start Pes Vm.4.4#0 on localhost :

FA364908

EcoStruxure Hybrid DCS [2018]- Virtualization Application Note

FA366094

EcoStruxure Hybrid DCS [2018]: Changing a controllers configuration without stopping the controller

FA364057

EcoStruxure Hybrid DCS[2018]: Error while starting Virtual Machine" Pes.Vm.4.4#0 on localhost or System.InvalidOperationException" for HDCS 2018

FA362765

EcoStruxure Hybrid DCS[2018]: Does license of MMM 2017 library work for MMM 2018 version

Video FAQs: NEW

FA361216

EcoStruxure Hybrid DCS [2018]- What is Role Base Access Control and how it works in Hybrid DCS 2018

FA361535

EcoStruxure Hybrid DCS [2018]: Video - How to configure and poll RS232 slave devices from NOM modules in multiple ERIO M580 drops

FA364063

EcoStruxure Hybrid DCS [2018] How do I navigate the EcoStruxure Hybrid DCS website?